• Home
  • Electronics Expo
  • Quality Articles
  • How to calculate Resistor Colour Code: Decoding Resistance Values

    Resistors are fundamental components in electronics, serving as passive elements that regulate the flow of electrical current. The ability to recognize their resistance value is crucial for anyone working with electronic circuits. This is where the resistor color code comes into play.

    To get the best quality resistors, you can order from WIN SOURCE. The company is one of the largest supplier of quality electronic components.

    Do you know how to calculate resistor codes? We will help you to learn to decode resistance values. Keep on reading .

    What is Resistor Color Code?

    The resistor color code is a system used to visually represent the resistance value of a resistor. This system utilizes colored bands placed on the body of the resistor to indicate the magnitude of its resistance.

    By understanding the color code, you can quickly determine the resistance value of a resistor without the need for complex measurements.

    How to Read Resistor Color Code?

    ● Observe the bands on the resistor’s body.

    ● Find the significant colors for digit representation.

    ● Match these colors to numbers and their positions.

    ● Read the digits left to right on the relevant band.

    First Band (Brown): Represents the first digit of the resistance value. In the case of 1k ohm, the first digit is 1.

    Second Band (Black): Represents the second digit of the resistance value. In this case, the second digit is 0.

    Third Band (Red): Multiplier band. This band determines the magnitude by which the first two digits should be multiplied. Red has a multiplier value of 100, so the multiplier for this resistor is 100.

    So, combining these colors, the 1k ohm resistor color code is Brown – Black – Red.

    1k ohm Resistor with 5 Bands: Resistors with 5 bands, such as the 1% tolerance resistors, provide even more precise resistance values. The first three bands determine the value, as explained above. The fourth band indicates the tolerance, which is crucial for ensuring the accuracy of the resistor’s value.

    What Does a 1k Resistor Look Like?

    A 1k ohm resistor, with a color code of Brown – Black – Red, is a standard resistor that can be found in various electronic circuits. It’s a through-hole component with color bands that uniquely identify its resistance value.

    This type of resistor helps regulate current flow while maintaining the desired voltage levels in a circuit.

    How is a 3.9 K Resistor Color Code?

    For a 3.9 K ohm resistor, the color code follows a similar pattern:

    ● First Band (Orange): Represents the first digit, which is 3.

    ● Second Band (White): Represents the second digit, which is 9.

    ● Third Band (Red): Multiplier band, with a value of 100.

    ● Fourth Band (Brown): Tolerance band, indicating a standard tolerance level.

    Anyone working with electronic circuits needs to know the resistor color code. It simplifies the selection of resistors for specific applications.  So that you can work efficiently and accurately.

    Are you looking for quality resistors? WIN SOURCE offers different types of resistors. You can select from renowned manufactures. Check out here to order now.