Feeling overwhelmed by connector chaos? Struggling to balance security and efficiency in your integration landscape? The CST 1130R-07 connector housing is what you need. This powerful rectangular housing connector paves the way for simpler, safer connector integration, letting you focus on what truly matters: unlocking the full potential of your data.
Let’s dig deeper and learn more.
What is a Rectangular Connector Housing?
A rectangular connector housing is a fundamental component in electronic systems, providing a protective enclosure for electrical connections. As the name suggests, it typically has a rectangular shape, offering a structured and organized framework for various connectors within.
This housing plays a crucial role in safeguarding delicate components from external elements, ensuring reliable and secure connections. Additionally, the rectangular design often facilitates straightforward integration into circuit boards, contributing to the overall efficiency and neatness of electronic assemblies.
These housings come in diverse sizes and configurations, catering to the specific needs of different connectors and applications in the electronic landscape.
CST 1130R-07 Connector Housing Overview
The CST 1130R-07 connector housing offers a compact and robust solution for electronic connections. Let’s break down the key specifications to understand its capabilities better.
1. Operating Temperature Range: -40℃~+105℃
One of the standout features of the CST 1130R-07 connector housing is its impressive operating temperature range. With the capability to function in temperatures ranging from -40℃ to +105℃, this connector is well-suited for a wide array of environments. Whether deployed in extreme cold or hot conditions, the CST 1130R-07 ensures reliable performance, making it a versatile choice for diverse applications.
2. Reference Series: A Legacy of Excellence
The CST 1130R-07 is part of a reference series known for its excellence in connector design. The reference series serves as a benchmark for quality and performance, and the CST 1130R-07 lives up to this legacy. When integrating connectors into your electronic systems, opting for a trusted reference series can instill confidence in the reliability and longevity of your connections.
3. Number of PINs Per Row: 7
The CST 1130R-07 features seven pins per row, providing ample connectivity options for a range of applications. This configuration strikes a balance between compactness and functionality, making it suitable for devices with space constraints while still meeting the connectivity requirements of most electronic systems.
4. Row Spacing: Single Row Configuration
Designed with simplicity in mind, the CST 1130R-07 features a single-row configuration. This design choice streamlines the integration process, simplifying the alignment and connection of the connector within your electronic setup. The single-row configuration also contributes to the overall compactness of the connector, making it suitable for applications where space is at a premium.
5. Pitch: 2mm
The 2mm pitch of the CST 1130R-07 is a key factor in its adaptability to various applications. The pitch, representing the distance between adjacent pins, strikes a balance between density and accessibility. This makes the CST 1130R-07 suitable for applications where a moderate pin density is required without compromising on ease of connection and accessibility.
6. Holes Structure: 1x7P
The hole structure of 1x7P refers to the arrangement of the connector pins. In this case, the CST 1130R-07 features a single row with seven pins. This configuration is a practical choice for applications where a specific number of connections is required, offering a standardized layout that simplifies both design and assembly processes.
Streamlining Integration: The Advantages of CST 1130R-07
Now that we comprehensively understand the CST 1130R-07’s specifications, let’s explore how these features translate into tangible benefits for connector integration.
1. Simplicity in Design and Assembly
The CST 1130R-07’s single-row configuration and 2mm pitch contribute to the simplicity of its design and assembly. Designers and engineers appreciate the straightforward layout, which reduces the complexity of integrating the connector into circuit boards and electronic systems. This simplicity not only accelerates the design process but also minimizes the chances of errors during assembly.
2. Versatility Across Applications
The broad operating temperature range of -40℃ to +105℃ ensures that the CST 1130R-07 can be deployed in various applications. Whether it’s in automotive electronics exposed to extreme temperature fluctuations or industrial equipment operating in harsh environments, the connector maintains its performance and reliability. This versatility makes the CST 1130R-07 a go-to choice for engineers working on projects with diverse application requirements.
3. Compact Footprint for Space-Efficient Designs
Combining a single-row configuration, 2mm pitch, and seven pins per row results in a compact footprint for the CST 1130R-07. This is particularly advantageous in applications with limited space, such as in consumer electronics or miniaturized devices. The connector’s compact design allows for efficient use of space on circuit boards without compromising on connectivity, making it an ideal choice for modern, sleek electronic designs.
Future-Proofing Your Designs with CST 1130R-07
As technology evolves, electronic components must keep pace with the changing landscape. The CST 1130R-07 meets current connectivity needs and future-proofs your designs in several ways.
1. Compatibility with Standardized Designs
As part of a reference series, the CST 1130R-07 aligns with industry standards, ensuring compatibility with various components and systems. This compatibility is crucial for future upgrades or modifications to electronic designs, allowing engineers to adapt to changing requirements without requiring a complete redesign.
2. Robust Construction for Long-Term Durability
The CST 1130R-07’s robust construction, coupled with its secure locking mechanism, ensures long-term durability. As electronic devices become integral to our daily lives, the demand for reliable and durable components increases. The CST 1130R-07’s ability to withstand challenging environmental conditions and maintain secure connections over time contributes to the longevity of electronic systems.
3. Adaptability to Emerging Technologies
With technological advancements, new applications and devices emerge, often with unique connectivity requirements. The CST 1130R-07, with its versatile design and reliable performance, can adapt to the evolving landscape of emerging technologies. Whether it’s about the Internet of Things (IoT), autonomous vehicles, or smart infrastructure, the CST 1130R-07 provides a solid foundation for future innovations.
Whether you are designing consumer electronics, automotive systems, industrial equipment, or any other electronic application, the CST 1130R-07 offers a balance of simplicity and performance.
Its adherence to industry standards, coupled with a legacy of excellence in the reference series, makes it a trusted choice for engineers and designers aiming to streamline connector integration and ensure the longevity of their electronic systems.
If you’re looking for top-notch connector housings, your next stop should be WIN SOURCE. They’re like a treasure chest for electronic components, offering a wide array of reliable and quality parts to complement the efficiency of connectors like the CST 1130R-07.
© 2025 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS