Resistors And Their Role in Electronics
A resistor is an electrical component that limits or controls the flow of electric current in a circuit. It does so by providing resistance to the flow of electricity, hence its name.
Resistance is measured in Ohms (Ω) and determines how much current can pass through a resistor. The higher the resistance, the lower the current that can pass through it. This makes resistors essential in regulating and protecting electronic circuits from damage caused by excessive current flow.
TubeDepot 273-39-RC Resistors
TubeDepot is a well-known brand among electronic enthusiasts and hobbyists for its high-quality components. Their 273-39-RC resistor is no exception. This through-hole resistor is made using metal film technology, which offers high accuracy and stability in its performance.
The 273-39-RC resistor has a resistance of 39Ω and can handle a power rating of 500mW. This makes it suitable for many low-power applications, especially in audio circuits where precision in resistance is crucial. The through-hole design also makes it easier to solder onto a circuit board, making it a popular choice among DIY electronics enthusiasts.
SMD Resistors
Surface Mount Device (SMD) resistors, on the other hand, have become increasingly popular in recent years due to their compact size and versatility. Unlike through-hole resistors that have leads for easy soldering, SMD resistors are directly mounted onto the surface of a circuit board, hence their name.
SMD resistors come in different sizes and shapes, making them suitable for various applications. They are also available in different technologies, including metal film, thick-film, and thin-film. However, their smaller size means they have a lower power rating compared to through-hole resistors.
The Difference Between TubeDepot 273-39-RC and SMD Resistors
Now that we have a basic understanding of both TubeDepot 273-39-RC and SMD resistors, let’s take a closer look at the differences between these two types.
Construction
The most apparent difference between these two types of resistors is their construction. As mentioned earlier, the 273-39-RC is a through-hole resistor, while SMD resistors are surface mount devices. This difference in construction has implications for their size and shape, as well as how they are mounted onto a circuit board.
Size and Footprint
As expected, due to their construction, TubeDepot 273-39-RC resistors are larger than SMD resistors. The through-hole design allows for more space, making it easier to manufacture and handle these resistors. In contrast, the compact size of SMD resistors makes them ideal for smaller electronic devices or densely packed circuit boards.
Moreover, the difference in size also affects the footprint of these resistors on a circuit board. Through-hole resistors have leads that need to be inserted into holes on the board, while SMD resistors are directly mounted onto the surface. This means that through-hole resistors take up more space on a circuit board compared to their SMD counterparts.
Power Rating
Another significant difference between TubeDepot 273-39-RC and SMD resistors is their power rating. The 273-39-RC can handle a power rating of 500mW, whereas SMD resistors have a lower power rating due to their smaller size. This means that through-hole resistors are better suited for high-power applications, while SMD resistors are more suitable for low-power circuits.
Temperature Coefficient
Temperature coefficient is another crucial difference between these two types of resistors. It refers to how a resistor’s resistance changes with temperature. TubeDepot 273-39-RC resistors have a low temperature coefficient, which means their resistance remains relatively constant even with changes in temperature.
On the other hand, SMD resistors can have higher or lower temperature coefficients depending on the technology used in their construction. This makes them ideal for certain applications, such as temperature sensing circuits.
Cost
Cost is always a factor to consider when choosing electronic components. In general, SMD resistors tend to be more cost-effective compared to through-hole resistors. This is due to their smaller size and ease of manufacturing, making them a popular choice in mass-produced electronics.
All in all, both TubeDepot 273-39-RC and SMD resistors have their own unique characteristics and advantages. While through-hole resistors offer higher power ratings and stability in performance, SMD resistors are more versatile and cost-effective. The choice between these two types ultimately depends on the specific needs of a circuit or project.
If you’re looking to purchase through-hole or SMD resistors, a reliable distributor like WIN SOURCE can provide you with high-quality components at competitive prices. They offer a wide range of electronic components from top brands, ensuring that you have access to the best options for your projects.
© 2025 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS