Electronic components are continuously evolving, and today, many switch types are available, each designed for specific functions. However, snap switches have notably become popular since their debut in 1932. They feature a durable design, ensuring prolonged longevity and resilience against challenging environmental conditions.
In addition, snap switches are compact, making them particularly well-suited for applications with limited space. Their swift response time is also invaluable for safety mechanisms and emergency shut-offs.
This article further delves into the details of snap switches, their types, working, and more. Continue reading!
What is a Snap Switch?
Snap switches are electrical switches that quickly transition from open to closed as pressure is applied to their actuator. The rapid response, accompanied by an audible “snap” sound as the contacts move between the on and off positions, makes them quite popular.
Snap switches find applications in electronics, where rapid and reliable switching is essential. They often feature a compact design, durability, and versatility, making them integral components in many electronic devices and systems.
Components of a Snap Switch
Let’s look at the components of a snap switch:
Actuator: It’s part of the switch that receives physical input, such as a button or lever, initiating the switching action.
Contacts: Conductive elements within the switch that make or break the electrical connection, determining the on/off state.
Snap Mechanism: The mechanism responsible for the rapid and distinctive switching action, often producing an audible “snap” when the contacts change position.
Terminals: Points on the switch for connecting electrical wires, facilitating the integration of the switch into an electrical circuit.
Working of Snap Switches
Here’s an overview of the working of a snap switch:
Start by pushing or pressing the actuator, the external part of the snap switch.
The applied pressure triggers a rapid movement of internal components known as contacts.
As the contacts move, they join, completing the electrical circuit and allowing the flow of electric current.
During this process, there is often a noticeable “snap” sound and tactile feedback, indicating the switch has changed state.
Releasing the pressure on the actuator returns the switch to its original state.
Types of Snap Switches
The most common types of snap switches are discussed below:
Actuator Styles
Here are some snap switch types as per the style of actuator:
Lever Snap Switch
A snap switch with an actuator in a lever facilitates manual operation by pushing or moving the lever. They are suitable for manual operation, such as control panels and machinery interfaces.
Plunger Snap Switch
A snap switch employing a plunger-style actuator, usually a push button-like component pressed to initiate the switching action. They are commonly found in devices and systems requiring a push-button mechanism, including electronic appliances, equipment, and safety systems.
Pole Styles
Common types of snap switches, depending upon their pole styles, are:
Double Pole Single Throw (DPST)
This snap switch configuration consists of two contacts that simultaneously open or close with a single actuation. DPST is suitable where you require the control of two separate electrical circuits.
Single Pole Double Throw (SPDT)
DPST snap action switches feature four terminals, functioning as two independent switches controlled by a single actuator. This design proves beneficial in situations demanding simultaneous control of two circuits, ensuring coordinated operation. They are frequently employed in industrial machinery and control panels for their versatile application.
Best Snap Switch Options Available
Here are some of the best snap switches available that you can try for various applications:
SS-5GL111D
The Omron Electronics Inc-EMC Div SS-5GL111D is a reliable switch with a voltage rating of 125V and a current rating of 5A (AC). It is designed for diverse electronic applications and offers a mechanical life of 30,000,000 cycles, making it an ideal, high-quality choice for various electronic devices.
1DM401
This snap switch 1DM401 features a robust 10A (AC) current rating, ensuring steadfast power delivery across various applications. Its 125V (AC) voltage rating accommodates diverse power requirements, making it suitable for residential and industrial use.
AV4524
The Panasonic Electric Works AV4524, part of the AV4 series, is a precision limit switch with a PC Pin termination style and a right-side mounted lever actuator. With a 30V voltage rating and SPDT circuit, this switch offers an On-Mom switch function. It boasts an electrical life of 20,000 cycles and a mechanical life of 300,000 cycles.
SDS001R
The C&K SDS001R is a compact surface-mount switch with a 100mA (DC) current rating and a 12V DC voltage rating. Featuring an SPST-NO circuit, an Off-Mom switch function, and an overtravel plunger actuator, it offers reliable performance in a compact design with 50,000 cycles of electrical and mechanical life.
Benefits of Snap Switches
Some expected benefits of snap switches are:
Rapid and Precise Switching
Snap switches are renowned for quick response time, allowing for swift and precise electrical switching. This attribute is crucial in applications where immediate and accurate control is required, enhancing the overall efficiency of electronic systems.
Reliability and Longevity
Snap switches are built using durable material and can easily withstand multiple mechanical actuations. This reliability is especially valuable in critical applications, ensuring consistent and trustworthy switching when essential.
Cost-Effectiveness
Snap switches offer a cost-effective solution for electronic switching needs. Their efficient design and long-lasting performance provide value for money in terms of initial investment and maintenance. This cost-effectiveness makes snap switches a preferred choice for various applications, balancing functionality and affordability in electronic systems.
Snap switches are reliable and employed in multiple applications, from control panels to safety systems and other electronics. They are budget-friendly and offer you a click or feedback when pressed. However, plenty of fake snap switches are available in the market, and finding the best snap switches is a hassle. In case you are in this situation, WIN SOURCE has you covered.
We have an extensive network of electronic components manufacturers and help your business connect with the most authentic ones. We are one of the best electronic components distributors and ensure you get your hands on high-quality snap switches through our network. Contact us today to experience unmatched performance, reliability, and quality.
© 2024 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS