Are you an average Joe who isn’t very familiar with technical lingo? Do you easily get lost when seeing random numbers and letters on a product name or label, especially on electronic parts and components? One such technical label you might have encountered is 200/12, sometimes written 200-12.
If you are wondering about this label, we will help you explore what it means and how it is used in electronic devices.
What is 200/12 on Electronic Product Names and Labels?
The 200/12 (or 200-12) stands for 200W and 12V, respectively. It indicates the power rating and voltage of a particular electronic component or device. The power rating refers to the maximum amount of power the component or device can handle without getting damaged. The voltage rating, however, refers to the amount of voltage the component or device requires to operate correctly.
It is essential to note that this specific label is just one example of a technical label you might encounter. Other labels might include different values, such as 100/24, 300/5, or 150/36. Each label represents a specific power rating and voltage requirement, depending on the device or component’s intended use.
Common Devices that are Manufactured with 200/12 Label
Now that we understand 200/12 let’s examine some common devices manufactured with this label.
Security Cameras
Many security cameras require a power supply that provides this specific amount of power. Many of the security cameras you find in establishments probably have this label. This label lets the camera operate reliably and capture high-quality footage without issues.
Computer Monitors
Computer monitors are another common device that often requires 200/12 power. This allows the monitor to display clear and vibrant images while ensuring that it runs smoothly without any issues. However, remember that not all computer monitors have this; some might have lower or higher labels.
LED Lighting Systems
LED lighting systems are becoming increasingly popular in homes and businesses worldwide. These systems often need this power label to operate effectively and provide bright, energy-efficient lighting.
Audio Amplifiers
Audio amplifiers increase the volume of audio signals. They are often used in home theaters, music, and sound systems. This power combination is commonly used in audio amplifiers, as it provides stable power to the amplifier without any distortion.
Medical Equipment
Several medical devices, such as blood glucose meters, nebulizers, and pulse oximeters, require a low voltage of 12 volts to operate. A 200/12 transformer can provide the necessary voltage to power these devices.
Industrial Machinery
Manufacturing facilities and other industrial settings often rely on machinery that requires this label. This includes everything from conveyor belts and assembly line machines to robotic arms and welding equipment.
Electric Motors
Electric motors are used in many industrial applications, such as manufacturing, construction, and transportation. Many electric motors require a low-voltage power supply, making them compatible with a 200/12 rating.
Telecommunications Equipment
Finally, many types of telecommunications equipment use this voltage combination to operate properly. This includes everything from routers and switches to phone systems and modems.
Take note that these are just a few examples of common devices manufactured with 200/12. Many other electrical devices require this voltage to function properly. Knowing a device’s voltage requirement is essential in ensuring that it is compatible with the electrical system in residential, industrial, or commercial buildings.
Safety Precautions When Handling 200/12 Devices
It is crucial to take the necessary safety precautions when handling devices that use electronic components with this label. Here are some tips to keep in mind:
- Always read the manufacturer’s instructions carefully before using the device.
- Ensure the device is unplugged from the power source before attempting to repair or replace any components.
- When handling electronic components, such as gloves and safety glasses, wear appropriate protective gear.
- Do not attempt to repair or replace any components if you are not qualified.
- If you notice any signs of damage or overheating, stop using the device immediately and seek professional help.
Understanding technical labels such as 200/12 is essential when using electronic devices safely. The label indicates a particular component or device’s power rating and voltage requirements and is used in a wide range of products.
Moreover, if you are looking for electronic components with this specific label, you can find them at WIN SOURCE. As an online electronic parts store that offers over a million obsolete and regular parts, we are a certified electronic components seller that ensures a 3-year guarantee of our products. Check out our website today to find the components you need for your next project.
© 2024 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS