![]() Figure 1 M25P16-VMC6TG device package |
![]() Figure 2 M25P16-VMC6TG schematic symbol |
What is M25P16-VMC6TG?
The M25P16-VMC6TG is an 16Mb (2Mb x 8) serial Flash memory device. M25P16-VMC6TG can be interfaced to microcontroller or microcomputer as DATA Storage.
Some of the essential features of M25P16-VMCT6TG are described below,
- Advanced Write Protection
- BULK ERASE Command: using it entire memory can be erased.
- SECTOR ERASE Command: using it one sector can be erased.
Pin Configuration
| PIN NO. | LABLE | TYPE | DESCRIPTION | |
| 1 | HOLD# | Input | Hold: The HOLD# signal is used to pause any serial communications with the device without deselecting the device. During the hold condition, DQ1 is High-Z. DQ0 and C are “Don’t Care.” To start the hold condition, the device must be selected, with S# driven LOW. | |
| 2 | VCC | Power | Device core power supply: Source voltage | |
| 3-6,11-14 | DNU | – | Do not use. | |
| 7 | S# | Input | Chip select: When the S# input signal is HIGH, the device is deselected and DQ1 is at high impedance. Unless an internal PROGRAM, ERASE, or WRITE STATUS REGISTER cycle is in progress, the device will be in the standby power mode (not the deep powerdown mode). Driving S# LOW enables the device, placing it in the active power mode. After power-up, a falling edge on S# is required prior to the start of any command. | |
| 8 | DQ1 | Output | Serial data: The DQ1 output signal is used to transfer data serially out of the device. Data is shifted out on the falling edge of the serial clock (C). | |
| 9 | W#/Vpp | Input | Write protect: The W#/Vpp signal is both a control input and a power supply pin. The two functions are selected by the voltage range applied to the pin. If the W#/VPP input is kept in a low voltage range (0 V to VCC) the pin is seen as a control input. The W# input signal is used to freeze the size of the area of memory that is protected against program or erase commands as specified by the values in BP2, BP1, and BP0 bits of the Status Register. VPP acts as an additional power supply if it is in the range of VPPH, as defined in the AC Measurement Conditions table. Avoid applying VPPH to the W#/VPP pin during a BULK ERASE operation. | |
| 10 | Vss | Ground | Ground: Reference for the VCC supply voltage. | |
| 15 | DQ0 | Input | Serial data: The DQ0 input signal is used to transfer data serially into the device. It receives commands, addresses, and the data to be programmed. Values are latched on the rising edge of the serial clock (C). | |
| 16 | C | Input | Clock: The C input signal provides the timing of the serial interface. Commands, addresses, or data present at serial data input (DQ0) is latched on the rising edge of the serial clock (C). Data on DQ1 changes after the falling edge of C. | |
Features
- 16Mb Flash memory
- single supply voltage: 2.7V to 3.6V
- Erase capability (Sector erase & Bulk erase)
- Write protection
- Deep power down: 1µA
- Maximum clock frequency: 75 MHz
- More than 20 years data retention
Applications
- Embedded system
- Camera device
ALTERNATIVES OF M25P16-VMC6TG
If you are looking for 16Mb Serial Flash Embedded Memory, here are some alternatives,
| 16MB SERIAL FLASH EMBEDDED MEMORY | ||
| PART NO. | SUPPLY VOLTAGE | CLOCK FREQUENCY |
| W25Q16JVSNIQ | 2.7V ~ 3.6V | 133MHz |
| MX25V1635FM1I | 2.3V ~ 3.6V | 80MHz |
| MX25R1635FZUIL0 | 1.65V ~ 3.6V | 33MHz |
WHERE TO USE M25P16-VMC6TG?
M29320DT Flash memory is a non-volatile memory chip used for storage and for transferring data between a personal computer (PC) and digital devices. It has the ability to be electronically reprogrammed and erased. It can be used in USB flash drives, MP3 players, digital cameras and solid-state drives.
How M25P16-VMC6TG work?

2-D VIEW OF M25P16-VMC6TG

Figure 3 2-D VIEW



COMMENTS