• Home
  • Parts Library
  • TUSB321AIRWBR

    Overview

    TUSB321AIRWBR is a USB Type-C port controller launched by Texas Instruments, suitable for various devices supporting USB Type-C interface. The device supports bidirectional USB Type-C connection and has efficient power transmission and data communication capabilities, which is very suitable for USB connection applications in consumer electronics, portable devices, and industrial automation.

    Core parameters

    parameter

    value

    Function

    USB Type-C Port Controller

    Operating voltage range

    3.0V to 5.5V

    Support Agreement

    USB Type-C 1.2

    Working Mode

    DFP/UFP/DRP

    Package Type

    WQFN-12

    Temperature range

    -40°C to 85°C

     

    Features and Benefits of TUSB321AIRWBR

    • Support multiple connection modes

    TUSB321AIRWBR supports USB Type-C bidirectional insertion function and has three operation modes: DFP (downstream port), UFP (upstream port) and DRP (dual role port). This enables it to flexibly adapt to different device connection requirements and play a role in various application scenarios.

    • Low power design

    The low-power design of the TUSB321AIRWBR is ideal for battery-powered and portable devices, providing efficient USB connectivity and communication capabilities while saving energy.

    • Flexible power management

    The device supports USB Power Delivery, which automatically adjusts the power supply according to the different needs of the connected device to ensure efficient power transmission. This is especially useful for devices that require high-power charging, such as laptops or portable displays.

    • Integrated overvoltage protection

    To ensure stable operation of the device, the TUSB321AIRWBR also has an integrated overvoltage protection function that can automatically protect the device from damage when the voltage exceeds the safe range.

    Application Areas

    • Consumer Electronics Devices

    TUSB321AIRWBR is widely used in consumer electronic devices such as laptops, tablets, and smartphones. It supports USB Type-C bidirectional insertion and efficient power transmission, which can improve the ease of use and charging efficiency of the device.

    • Industrial Automation Equipment

    In industrial automation equipment, the rugged design and versatility of the TUSB321AIRWBR can meet the requirements of harsh working environments and provide stable USB connection and data transmission capabilities for the equipment.

    • Portable Devices

    The low power design of the TUSB321AIRWBR is particularly suitable for portable devices such as portable chargers, displays, and storage devices. In these applications, it can ensure efficient energy transfer and long-term device operation.

    Competitive Analysis: TUSB321AIRWBR vs. Other USB Port Controllers

    Compared with other USB Type-C port controllers on the market, the advantage of TUSB321AIRWBR is that it supports multiple operation modes and USB Power Delivery functions. It not only has efficient power management functions, but also ensures stable operation of devices in complex environments.

    Features/Specifications

    TUSB321AIRWBR

    Other USB Type-C Controllers

    Support Mode

    DFP/UFP/DRP

    Only supports DFP or UFP

    Power Delivery

    Supports USB Power Delivery

    Not supported

    Package Type

    WQFN-12

    QFN, WQFN

    Power consumption

    Low power design

    Standard power consumption

     

    Why choose TUSB321AIRWBR?

    The TUSB321AIRWBR’s versatility, low-power design, and efficient power management make it an ideal choice for USB Type-C connected applications. Whether in consumer electronics, industrial automation, or portable devices, the TUSB321AIRWBR provides stable performance, enhanced power delivery, and superior safety.

    FAQ

    Q1: How does TUSB321AIRWBR support USB Power Delivery?
    TUSB321AIRWBR supports USB Power Delivery (PD) protocol, which dynamically adjusts power delivery to meet the power requirements of different devices. This feature enables it to provide fast charging when the device has high power requirements, such as providing stable power supply for devices such as laptops and high-power monitors, while ensuring efficient and safe power delivery.

    Q2: What are the advantages of the TUSB321AIRWBR package type?
    TUSB321AIRWBR adopts WQFN-12 package. Its compact design not only saves circuit board space, but also has good heat dissipation performance, which is suitable for high-density design. This package type also improves the mechanical strength and reliability of electrical connections, allowing the device to maintain stable performance in harsh application environments, suitable for industrial and consumer electronics applications.

    For more details and to explore our inventory, please visit the links below:

    Product Details: Win Source – TUSB321AIRWBR
    Price: Win Source – RFQ for TUSB321AIRWBR

    ©2024 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0