• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • According to the characteristics and applications of each stage of FPGA development, what can be divided into?

    * Question

    According to the characteristics and applications of each stage of FPGA development, what can be divided into?


    *
    Answer

    According to the characteristics and applications of each stage of FPGA development, it can be divided into 3 generations.The first generation of FPGA devices is called a logic-level FPGA device.Second-generation FPGA devices have system integration capabilities called system-level FPGA devices.

    Integrating a variety of IP soft cores and hard cores reduces system development time. A single platform FPGA can integrate multiple applications. The FPGA devices at this stage are called platform-level FPGA devices, that is, third-generation FPGA devices.