* Question
Is it true that digital control typically refers to one of three primary control architectures?
* Answer
Yes — that’s correct. In power electronics and embedded systems, when people refer to digital control, they usually mean one of three primary control architectures. Each has different levels of flexibility, complexity, and performance:
Table of Contents
Toggle1. Fully Digital Control
Description:
Both the control algorithm and signal processing are executed in the digital domain by a microcontroller, DSP, or FPGA.
Feedback signals are digitized by ADCs and processed using software or programmable logic.
Advantages:
Maximum flexibility — control laws can be updated or reprogrammed.
Supports advanced algorithms (adaptive control, nonlinear control, predictive models).
Applications:
High-performance motor drives.
Digital power converters (server power supplies, telecom systems).
2. Analog Control with Digital Supervisory
Description:
The main control loop (feedback, compensation) is implemented in analog circuitry (op-amps, comparators).
A digital controller (MCU, PMBus, I²C interface) provides supervisory functions like monitoring, trimming, fault handling, or mode switching.
Advantages:
Combines the fast response of analog control with digital programmability.
Lower cost than fully digital solutions.
Applications:
Power management ICs (PMICs).
Simple regulators with digital configurability.
3. Hybrid / Mixed-Signal Control
Description:
Core control functions (e.g., error amplification, PWM generation) are digital, but some elements remain analog (such as current sensing or high-speed comparators).
Often implemented in mixed-signal controllers or digital power ICs.
Advantages:
Balance between speed, precision, and flexibility.
Easier migration path from traditional analog to full digital.
Applications:
Point-of-load regulators.
Automotive power systems.
Summary
Yes — digital control in practice usually refers to one of three architectures:
Fully digital control (all in software/logic).
Analog control with digital supervisory functions.
Hybrid / mixed-signal control (shared analog and digital tasks).
This classification helps engineers pick the right balance of speed, programmability, cost, and complexity for their design.

COMMENTS