* Question
Embedded system hardware initialization is divided into several links?What is it?
* Answer
Embedded system hardware initialization typically consists of several stages or steps, often referred to as “links.” These stages ensure that the hardware is properly set up and ready to execute higher-level software, such as the operating system or application code. Here are the key stages involved:
1. Power-on Reset (POR)
– This is the initial stage where the hardware system comes to life after power is applied. The system generates a reset signal to ensure all hardware components start from a known state. During this phase, voltage levels are stabilized, and the system clock starts running.
2. Bootloader/Startup Code Initialization
– The bootloader is the first piece of code executed after reset. It performs essential initialization tasks, such as setting up the stack pointer, initializing the memory (RAM), and configuring the processor’s operating modes. The bootloader may also load the operating system or application code into memory and pass control to it.
3. Hardware Component Initialization
– In this stage, critical hardware components such as timers, interrupts, UARTs, I2C/SPI interfaces, and GPIOs are initialized. This is required to ensure all hardware peripherals function correctly for subsequent operations. Device-specific drivers often perform this task.
4. Memory Setup
– The system configures both volatile (RAM) and non-volatile memory (such as Flash or EEPROM). This ensures that memory regions are mapped correctly, stack and heap are set, and that critical memory spaces are allocated for system functions.
5. Processor Configuration
– The CPU and co-processors are configured. This includes setting up processor registers, configuring operating modes (user/supervisor modes), setting up caches, and enabling hardware-specific features like power-saving modes.
6. Interrupt System Initialization
– Interrupt controllers and the interrupt vector table are set up, enabling the system to handle interrupts efficiently. Proper interrupt handling is crucial for real-time responses in embedded systems.
7. Peripheral Initialization
– Additional peripherals such as sensors, actuators, communication interfaces, and custom hardware modules are initialized. Peripheral drivers are loaded, and any required communication protocols (e.g., USB, Ethernet) are enabled.
8. Application-Specific Initialization
– Finally, the system initializes application-specific modules and settings, such as setting timers for task scheduling, starting real-time operating systems (RTOS), or loading specific application logic.
Each of these stages is vital to ensuring that the embedded system operates correctly and reliably. Skipping any of these steps can result in improper functioning or failure of the system.

COMMENTS