* Question
From a programming point of view, what are the working states of ARM microprocessors?
* Answer
From a programming perspective, ARM microprocessors operate in several working states, which define the execution mode and behavior of the processor. These states can be categorized into processor modes, instruction set states, and execution states. Understanding these states is crucial for effective programming and system-level design.
1. Processor Modes
The processor mode determines the privilege level and the resources available to the processor. ARM processors support several modes, primarily divided into privileged and non-privileged modes.
Privileged Modes
These modes allow full access to system resources and are typically used by the operating system or exception handlers:
– Supervisor Mode (SVC): Entered on reset or when a software interrupt (SWI) occurs. Used for OS-level operations.
– Abort Mode (ABT): Used to handle memory access violations (e.g., prefetch or data aborts).
– Undefined Mode (UND): Activated when the processor encounters an undefined instruction.
– IRQ Mode (IRQ): Used for handling normal interrupt requests.
– FIQ Mode (FIQ): Used for handling fast interrupt requests with higher priority than IRQ.
– Monitor Mode: Used in TrustZone-enabled processors for secure world operations.
– Hyp Mode: Introduced in ARMv7-A for virtualization purposes (used by hypervisors).
Non-Privileged Mode
– User Mode: The default mode for application-level code. It has restricted access to system resources to ensure stability and security.
2. Instruction Set States
ARM microprocessors support different instruction sets, which determine how instructions are fetched and executed:
– ARM State: Executes 32-bit ARM instructions. This is the default state for most ARM processors.
– Thumb State: Executes 16-bit Thumb instructions, providing higher code density at the cost of reduced instruction complexity.
– Thumb-2 State: A hybrid of ARM and Thumb, offering both high code density and performance.
– Jazelle State: For executing Java bytecodes directly in hardware (optional feature in some ARM processors).
– ThumbEE State: An enhancement for Thumb, used in dynamically generated code or managed runtime environments.
The current instruction set state is indicated by the T-bit in the CPSR (Current Program Status Register):
– T-bit = 0: ARM state
– T-bit = 1: Thumb state
3. Execution States
The execution state defines the operating environment of the processor. ARM processors, particularly ARMv8 and later, support:
– AArch32: Executes 32-bit instructions and uses a 32-bit register set. Compatible with legacy ARM systems.
– AArch64: Executes 64-bit instructions and uses a 64-bit register set. Introduced in ARMv8 for higher performance and efficiency.
The current execution state is determined by the EL (Exception Level) and the processor configuration.
4. Exception Levels (ARMv8 and Later)
ARMv8 introduced Exception Levels (EL) to provide finer control over privilege and execution contexts:
– EL0: Non-privileged, used for user applications.
– EL1: Privileged, used for operating system kernels.
– EL2: Hypervisor level, used for managing virtual machines.
– EL3: Secure monitor level, used for TrustZone’s secure world operations.
5. Power States
ARM microprocessors also have power states to manage energy efficiency:
– Run State: The processor is fully powered and executing instructions.
– Idle State: The processor is not executing instructions but remains powered.
– Sleep State: Parts of the processor are powered down to save energy.
– Deep Sleep State: Most of the processor is powered down, retaining only essential states.
Summary
ARM microprocessors operate in a combination of working states that include:
1. Processor Modes: Define privilege levels and context (e.g., User, Supervisor, IRQ).
2. Instruction Set States: Determine the type of instructions being executed (e.g., ARM, Thumb).
3. Execution States: Define the operational bit-width and exception level (e.g., AArch32, AArch64).
4. Power States: Manage the energy consumption of the processor.
By leveraging these states, programmers can optimize ARM-based systems for performance, security, and power efficiency.

COMMENTS