* Question
How to use incremental encoders |
* Answer
1, incremental rotary encoder has a difference in resolution, using the number of pulses generated per revolution to measure, the number from 6 to 5400 or higher, the more the number of pulses, the higher the resolution; this is an important basis for selectionone.Generally, the A-pre-B or B-pre-A is used for judgment.
The incremental encoder of our company is defined as the shaft end seeing the encoder rotates clockwise to forward rotation, the A-pre-B is 90°, and the counterclockwise rotation is reverse B-out.A is 90°.There are also different ones, depending on the product description., set up a counting stack in the electronic device. |
COMMENTS