• Home
  • QUESTIONS & ANSWERS
  • Resistors
  • How to use the Resistors correctly?

    * Question

    How to use the Resistors correctly?

    * Answer

    1. Understand the Purpose of a Resistor

    Resistors are passive components that limit current, divide voltage, or provide biasing and load functions in a circuit. Before using one, clarify what role it plays:

    Current limiter (e.g., for LEDs)

    Voltage divider (e.g., scaling signals)

    Pull-up/pull-down resistor (e.g., in digital logic)

    Timing element (e.g., with capacitors in RC circuits)

    2. Select the Correct Resistance Value

    Use Ohm’s Law:

    R=V/I​

    where VVV is the voltage across the resistor and III is the desired current.

    Example: To limit an LED with 2 V drop at 20 mA from a 5 V supply:

    R=(5V−2V)/0.02A=150 Ω

    3. Check Power Rating

    Resistors convert excess energy into heat.

    Power is given by:

    P=V×I=I2×R=V2/R

    Always choose a resistor rated at least 2× the expected dissipation to avoid overheating.

    Common ratings: 1/8 W, 1/4 W, 1/2 W, 1 W, etc.

    4. Orientation and Placement

    Resistors are non-polarized — they can be placed in either direction.

    On PCBs, follow layout rules:

    Keep resistor leads short to minimize noise and inductance.

    Place current-limiting resistors close to the load (e.g., next to an LED).

    5. Use the Correct Tolerance

    Tolerance indicates how close the actual resistance is to the nominal value (e.g., ±1%, ±5%).

    Precision circuits (e.g., reference voltage dividers) require low tolerance (1% or better).

    General-purpose applications can use 5% or 10%.

    6. Special Applications

    Voltage Divider: Two resistors in series split voltage proportionally.

    Pull-up / Pull-down: Ensure logic inputs are in a defined state when not driven.

    Bleeder Resistors: Safely discharge capacitors in power circuits.

    Summary Table

    Step

    Key Consideration

    Define purpose

    Current limit, voltage divider, biasing, etc.

    Calculate resistance

    Use Ohm’s law (R = V/I)

    Check power rating

    Ensure ≥2× margin to avoid overheating

    Place correctly

    Non-polarized, but consider PCB layout

    Choose tolerance

    ±1% for precision, ±5–10% for general use

    Apply in circuits

    Voltage dividers, pull-ups, bleeders, LED limiting

    In short: Always calculate resistance with Ohm’s law, check the power rating, choose suitable tolerance, and place resistors with good layout practice.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0