• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is the sample rate set?

    * Question

    If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is the sample rate set?


    *
    Answer

    The sampling rate setting steps are as follows:

    (1) Enable and power up the ADC and DAC through registers 26h and 3Ch;

    (2) Enable register 2Ah bit [0]VRA;

    (3) Change the sample rate value in the respective registers.