• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • In the wake-up request, the transceiver asserts the pin INH output to activate the external supply voltage regulator.What events can I set pin INH to high?

    * Question

    In the wake-up request, the transceiver asserts the pin INH output to activate the external supply voltage regulator.What events can I set pin INH to high?


    *
    Answer

    1VBAT is powered up (cold start).

    2 pin WAKE rising or falling edge.The 3-pin EN or pin STB is low and the message frame has a dominant phase that is at least tCANH or tCANL maximum.4 When VCC is activated, pin STB goes high.