* Question What are the main parameters that wind turbines need to monitor? * Answer Wind speed, wind direction, wind…
* Question What stages can EC0 be applied to? * Answer EC0 can be mainly applied in the HDL phase…
* Question What are the codes for commonly used baseband digital signals? * Answer Commonly used baseband digital signal coding…
* Question What is key management? * Answer Key management is a comprehensive technology that involves the entire process of…
* Question What areas of wireless sensor network applications are currently concentrated? * Answer Environmental monitoring and protection, medical care,…
* Question What options does the 28x family of devices offer to generate clocks? * Answer Using the on-chip crystal…
* Question What are the disadvantages of LD0? * Answer The disadvantage of LD0 is its low efficiency and can…
* Question What is the test principle of COS? * Answer (1) The test requirements are detailed and comprehensive, and…
* Question What is the role of the source module? * Answer The purpose of the source module is to…
* Question What is the procedure for sending an address? * Answer Set TXWAKE = 1 and write the appropriate…