* Question What functions are completed by the substation inspection system based on sensor technology and RFID radio frequency identification…
* Question How to design a fast data exchange mechanism for multi-DSP digital controllers? * Answer Commonly used implementation methods…
* Question What are the TV encoder related registers? * Answer 1. TV Controller control SFR set 2. Vertical back…
* Question What are the main technical features of the MAX6966? * Answer 1 with high-speed 26MHz SPI / QSPI…
* Question The amount of information transmitted by the tag also directly affects the polling time.Therefore, what are the main…
* Question How to easily identify common varactor diodes? * Answer The varactor diode is a special diode specially designed…
* Question What are the three major categories of electrolytes for electric double layer capacitors? * Answer 1 water system;…
* Question What are the VHDL data objects of the combined circuit? * Answer 1) Constant 2) Signal 3) Variable
* Question Which two types of sensors are calibrated? * Answer The calibration of the sensor is divided into static…
* Question What are the main technical features of the MAX7316? * Answer 1400kbit/s, 2-wire serial interface, 5.5V voltage tolerance;…