* Question Capacitor detection method and experience * Answer 1. Detection of fixed capacitors.A. Detecting small capacitors below 10pF Because…
* Question What is a GPRS module? * Answer GPRS (General Packet Radio Service) is a new bearer service developed…
* Question What is the working principle of the OTL circuit? * Answer Complementary symmetrical power amplifiers are also known…
* Question What are the basic requirements for electrode materials for thermocouples? * Answer 1 In the temperature range, the…
* Question Briefly describe the pin function of the 100V flyback isolation controller – LT3748? * Answer (1) VIN (1PIN):…
* Question What is IEC 62026? * Answer IEC 62026 is the electrical interface standard for controllers used in low…
* Question The difference between an op amp and a comparator * Answer The op amp and the comparator are…
* Question What is the temperature difference potential? * Answer The electric field hinders the continued diffusion of electrons. When…
* Question What are the components of the microphone input? * Answer 1 microphone preamplifier 2 single microphone application 3…
* Question What are the features of the VIC module in the LPC2000 series ARM? * Answer (1) ARM PrimeCell…