* Question What is the role of the phosphorescent photosensitizer? * Answer The role of the phosphorescent photosensitizer is to…
* Question What are the important technical indicators of the successive approximation analog-to-digital converter? * Answer 1) Resolution, which is…
* Question What is the complement/reverse command?… * Answer H: X/SP increment instruction AIX/AIS is used to directly increase the…
* Question What are the two principles of oscillation blocking? * Answer The first type consists of four parts of…
* Question Why do capacitor applications have to be accompanied by Resistorss? * Answer A capacitor is an energy storage…
* Question What is a small-scale propagation model? * Answer The small-scale propagation model is used to describe the rapid…
* Question What is the basic magnetization curve?What is hysteresis loss? * Answer Basic magnetization curve—-The shape of the hysteresis…
* Question What are the main new features of SJAl000? * Answer 1 Standard frame format and extended frame format…
* Question What is the difference in the performance of the filter components? * Answer 1) Capacitor.It is used to…
* Question What are the jump instructions? * Answer 4 jump instructions: B, BL, BLX, HX