* Question The LM5070 is a very unique chip. What are the unique features? * Answer 1 Undervoltage lockout (UVLO)…
* Question What are the principles to follow for antenna selection? * Answer 1) Determine the density of different antenna…
* Question What are the commonly used radiant heat detectors? * Answer Commonly used radiant heat detectors include thermistor type…
* Question What components do the composite signals consist of? * Answer Luminance signal – contains the intensity (brightness or…
* Question What are the key components that need to be selected in the circuit design? * Answer (1) Clamping…
* Question What is SSDl355? * Answer SSDl355 is a 0LED color screen driver chip developed by Solomon Systech. The…
* Question What parameters are affected by the identification range? * Answer The identification range is one of the most…
* Question Compared with the international advanced level, what are the main gaps in the design of RFID chips in…
* Question What are the disadvantages of barcodes? * Answer • The barcode must face the scanner to successfully read…
* Question What is the load capacitance? * Answer Load capacitance is an extremely important parameter to describe the application…