* Question The thermoelectric potential generated in the thermocouple loop consists of two potentials? * Answer The thermoelectric potential generated…
* Question What are the VHDL finite state machines for sequential logic circuits? * Answer (1) Whether the output of…
* Question What is the main purpose of the switch output type liquid level sensor? * Answer Brake fluid level,…
* Question What is a counter? * Answer The counter consists of a programmable counter chip.Usually a 16-bit counter.Under the…
* Question What are the main technical features of MAXl707? * Answer 1) It can drive 4 white LEDs, each…
* Question How to distinguish between dry film and wet film? * Answer The dry film wet film basically functions…
* Question What are the advantages of displaying the battery status? * Answer a.The disconnection value can be set directly…
* Question What are the main applications of NTC and PTC thermistors? * Answer (I) Application in temperature measurement (II)…
* Question How to use incremental encoders? * Answer Incremental rotary encoder has a difference in resolution, using the number…
* Question What are the main components of the AC-Link output frame (SDATA_OUT)? * Answer AC-Link output frame (SDATA_OUT) is…