* Question What are the applications of automotive sensors? * Answer Air flow meter, pressure sensor, position sensor, speed sensor,…
* Question Which applications are considered for ZigBee technology? * Answer The equipment spacing is small; the equipment cost is…
* Question What are the most famous logic synthesis tools in FPGA/CPLD design? * Answer There are three most well-known…
* Question Several failure modes related to supercapacitors * Answer 1) The well-known bathtub curve reflects early failure and wear…
* Question What are the currently widely used stochastic mobile models based on independent and identical distribution? * Answer Random…
* Question Which instructions are included in the transfer class instruction? * Answer 1.Accumulator A compares equal branch instructions.Subtract l…
* Question What kinds of wireless communication technology can be divided into? * Answer Wireless personal area network, wireless local…
* Question What is the nature of the wiring pool? * Answer The so-called wiring pool is essentially a switch…
* Question What is a combiner? * Answer The main function of the combiner is to combine several signals from…
* Question Which roles do you need to define for devices that implement common attribute specifications? * Answer Client: Initiates…