* Question
| The early combinational logic circuit design was based on manual design. How to design by Boolean algebraic simplification? |
* Answer
| The first step is to convert the logical proposition of the text description into a truth table.First, analyze the causal relationship of the event and determine the input and output variables.Generally, the cause of the event is always defined as an input variable, and the result caused by the event is defined as an output variable.The third step is to draw a logic diagram and eventually convert it into a circuit. |

COMMENTS