* Question
Varistor parameters
* Answer
A varistor (variable resistor), also known as a voltage-dependent resistor (VDR), is an electronic component used to protect circuits from voltage surges. It has a nonlinear, non-ohmic current-voltage characteristic, meaning its resistance decreases with an increase in voltage. Here are the key parameters of a varistor:
Key Parameters of a Varistor
1. Varistor Voltage (V₁₀₀ₐ or V₅₀ₐ)
– Definition: The voltage across the varistor at a specified current, often 1mA (V₁₀₀ₐ) or 50µA (V₅₀ₐ).
– Importance: Indicates the voltage at which the varistor starts to conduct significantly, providing a measure of its operating voltage range.
2. Maximum Allowable Voltage (AC and DC)
– Definition: The maximum continuous voltage the varistor can withstand without significant degradation.
– Importance: Ensures the varistor can handle the normal operating voltage of the circuit.
3. Clamping Voltage (V_clamp)
– Definition: The voltage across the varistor when a specified peak pulse current is applied.
– Importance: Represents the voltage level that the varistor will clamp to during a surge, protecting the circuit.
4. Energy Rating (W₀ or E)
– Definition: The maximum energy the varistor can absorb in a single pulse without damage, usually specified in joules.
– Importance: Indicates the varistor’s ability to handle surge energy.
5. Peak Pulse Current (I_p or I_tm)
– Definition: The maximum peak current the varistor can handle in a single pulse without degradation.
– Importance: Defines the maximum surge current the varistor can safely conduct.
6. Response Time (t_r)
– Definition: The time it takes for the varistor to respond to a voltage surge.
– Importance: A fast response time ensures quick protection of the circuit.
7. Capacitance (C)
– Definition: The capacitance of the varistor, usually measured at a specific frequency and voltage.
– Importance: Affects the varistor’s performance in high-frequency applications and can influence circuit impedance.
8. Leakage Current (I_leak)
– Definition: The small current that flows through the varistor at a specified voltage below the varistor voltage.
– Importance: Indicates the amount of current that will leak in normal operating conditions, which should be minimal.
9. Operating Temperature Range
– Definition: The range of temperatures within which the varistor can operate without significant performance degradation.
– Importance: Ensures reliability and stability across different environmental conditions.
10. Life Expectancy and Degradation
– Definition: The expected operational life of the varistor under specified conditions, including the number of surge events it can endure.
– Importance: Provides an estimate of the varistor’s durability and longevity in protecting circuits.
When selecting a varistor for a specific application, it is crucial to consider these parameters to ensure proper protection of the circuit. The varistor should match the operating voltage range, handle expected surge currents and energy, respond quickly to surges, and maintain reliability over its intended lifespan.

COMMENTS