* Question
| What are the advantages of NiosII’s implementation of embedded systems? |
* Answer
| 1.The Benefits of a Configurable Soft Core Embedded Processor One of the biggest challenges faced by embedded developers is how to choose a processor that fits their application needs.Either in order to maintain the cost of the demand, the ideal plan originally expected is not achieved.With the introduction of the Nios II soft-core processor, engineers can easily create a “perfect” processor, regardless of peripherals, memory interfaces, performance characteristics, and cost..Delivering a Proper Performance Combination With Altera Nios II processors and FPGAs, designers can create a perfect solution for processors, peripherals, memory and I/O interfaces.
3.Improving system performance Embedded developers must choose a processor to determine the right system performance.The performance of the iOS II system can be tailored to the application, with higher performance at lower clock rates than fixed processors such as ARM processors.4.Reduce system costs Embedded designers are constantly looking for ways to reduce system costs. |

COMMENTS