* Question
| What are the advantages of using VHDL for engineering design? |
* Answer
| 1 Compared with other hardware description languages, VHDL has stronger behavior description ability, which determines it becomes the best hardware description language in system design field.Powerful behavioral description capabilities are important guarantees for avoiding specific device structures and describing and designing large-scale electronic systems from logical behavior.High-efficiency, high-speed completion of large-scale systems that meet market needs must be performed by multiple people or even multiple generations in parallel.
4 For a deterministic design done with VHDL, EDA tools can be used for logic synthesis and optimization, and the VHDL description design is automatically transformed into a gate-level netlist. |

COMMENTS