* Question
| What are the characteristics of Byteflight? |
* Answer
| (1) The bit transfer rate is 10 Mb/s, and the net data transfer rate is 5 Mb/s.(2) The maximum data refresh time is 250?s.
(3) The coding mode of the start bit and the stop bit of the NRZ band is adopted. (4) The protocol itself does not define a node number limit. (5) The protocol does not define the network topology. 9) Even if the bus is at maximum load, it can guarantee the timely transmission of a certain number of highest priority information, that is, the bus will not be “blocked” for the highest priority information. (10) When the bus load is low, low priority information can access the bus as if it were asynchronous. |

COMMENTS