* Question
| What are the characteristics of the parallel process program? |
* Answer
| A parallel flow program with three branches, the characteristics of which are as follows.
(1) If S20 has been operated, the three processes (S21, S22, S31, S32, S41, and S42) are simultaneously executed in parallel as long as the branch transition condition X0 is established, and there is no succession.In addition, parallelism flow programs may have two or more states in the “active” state at the same time. |

COMMENTS