* Question
What are the commonly used optical paths for gratings?
* Answer
In optical systems using diffraction gratings, the “optical path” refers to how light travels from the source, through the grating, and toward the detector. The arrangement determines resolution, efficiency, and application suitability.
Here are the commonly used optical path configurations for gratings:
Table of Contents
Toggle1. Littrow Configuration
Description: The incident and diffracted beams are aligned so that the diffracted light retraces the path of the incident light.
Advantages:
High efficiency because the blaze angle is optimized for the working wavelength.
Compact design.
Applications:
Tunable lasers
Wavelength selection systems
2. Ebert–Fastie Monochromator Path
Description: Light passes through an entrance slit, is collimated, diffracted by the grating, and then focused onto an exit slit by the same mirror system.
Advantages:
Simpler alignment
Cost-effective
Applications:
Medium-resolution spectrometers
3. Czerny–Turner Configuration
Description: Uses two separate mirrors—one for collimation before the grating and one for focusing afterward—keeping the entrance and exit slits on opposite sides.
Advantages:
Widely used in commercial spectrometers
Reduced optical aberrations compared to single-mirror setups
Applications:
UV–Vis–NIR spectroscopy
Analytical instruments
4. Off-Plane (Conical Diffraction) Configuration
Description: The incident light is not in the plane perpendicular to the grating grooves, producing conical diffraction.
Advantages:
Can handle high dispersion in compact geometry
Useful for extreme ultraviolet (EUV) and X-ray wavelengths
Applications:
Synchrotron beamlines
High-resolution spectroscopy
5. Rowland Circle Mount
Description: The entrance slit, grating, and detector are placed on the circumference of a Rowland circle defined by the grating’s radius of curvature.
Advantages:
Naturally corrects certain aberrations
Good for fixed-grating spectrometers
Applications:
Vacuum UV spectroscopy
Emission spectrometers
Summary Table
Optical Path | Main Advantage | Common Applications |
Littrow | High efficiency, compact | Tunable lasers, wavelength selection |
Ebert–Fastie | Simple, low-cost | Medium-resolution spectrometers |
Czerny–Turner | Low aberrations, versatile | UV–Vis–NIR spectrometers |
Off-Plane | High dispersion, compact | EUV/X-ray spectroscopy |
Rowland Circle | Aberration correction | UV & emission spectrometry |

COMMENTS