* Question
| What are the conclusions of the test analysis? |
* Answer
| (1) The level of the signal transmitted on the CAN bus of the body comfort system is consistent with the nominal value of the signal level defined by IS0. The data transmission rate is 62.5 kb/s, which belongs to Volkswagen’s second generation body comfort system.
3) CAN bus In the case of analog bus faults related to CAN-H and CAN-L short circuit and open circuit, the signals on the CAN bus can be transmitted in a single line mode, and the bus works in single line mode. |

COMMENTS