* Question
| What are the functions of each component of the PLC system? |
* Answer
| The basic unit (ie, the main unit) is the core of the PLC control; the expansion unit is a device that expands the number of I/O points, and has a power supply inside; the expansion module is used to increase the number of I/O points and the ratio of changing the number of I/O points, and there is no power inside.Powered by the base unit or expansion unit, the expansion unit and the expansion module have no CPU. |

COMMENTS