* Question
What Are the Functions of the Power Management Module in the BQTINY-11 System?
* Answer
The BQTINY-11 power management module belongs to the bqTINY series of lithium-ion battery charge management ICs designed for portable electronic devices such as smartphones, handheld equipment, and media players. These devices integrate battery charging control and system power-path management into a single chip, allowing the system to be powered while simultaneously charging the battery.
The power management module in BQTINY-11 performs several key functions that ensure safe battery charging, stable system power supply, and protection of the battery pack.
1. Three-Stage Automatic Charging Control
One of the core functions of the BQTINY-11 module is automatic three-stage charging management for lithium-ion batteries.
The charging process typically includes:
- Pre-charge (conditioning stage)– applied when the battery voltage is very low
- Constant-current (CC) charging– the battery is charged at a fixed current
- Constant-voltage (CV) charging– voltage is regulated while current gradually decreases
This charging profile protects the battery and maximizes battery life while ensuring efficient energy transfer.
2. Automatic Power Source Selection
The module supports automatic power supply selection between different input sources.
Typical sources include:
- AC adapter input
- USB power input
- Battery supply
The system can automatically switch to the appropriate source depending on availability. This power-path management ensures continuous system operation even when one power source becomes unavailable.
3. Battery Temperature Protection
The BQTINY-11 module includes battery temperature monitoring and protection mechanisms.
Using temperature sensing inputs, the system can detect when the battery becomes:
- Too hot
- Too cold
If the battery temperature moves outside the safe operating range, the charging process is automatically suspended to prevent battery damage or safety hazards.
4. Pre-Charging Mechanism for Deeply Discharged Batteries
When a lithium-ion battery is deeply discharged, normal fast charging could damage the cell.
To prevent this, the BQTINY-11 module implements a pre-charge (conditioning) stage that applies a small current to gradually restore the battery voltage before entering normal charging mode.
This feature improves both battery safety and recovery reliability.
5. Automatic Charging Voltage Regulation
The module maintains precise control over the charging voltage level during the constant-voltage phase.
Typical regulation voltages for Li-ion batteries include:
- 1 V
- 2 V
- 36 V
Accurate voltage regulation prevents overcharging and ensures optimal battery capacity and lifespan.
6. Charging Status Monitoring and Automatic Termination
The power management module also provides charging status monitoring and automatic charge termination.
When the battery becomes fully charged:
- The charging current falls below a preset threshold
- Charging is automatically terminated
If the battery voltage later drops below a certain level, the system can automatically restart the charging cycle, maintaining battery readiness.
7. Sleep Mode and Status Signal Output
To minimize power consumption when external power is removed, the BQTINY-11 module supports a sleep mode.
Additional features include:
- Charge status indicator outputs (often used to drive LEDs)
- Fault condition signaling to the system controller
These outputs allow the host system to monitor charging progress and detect abnormal conditions.
Conclusion
The BQTINY-11 power management module integrates multiple essential battery management functions into a single device. Its main capabilities include:
- Three-stage automatic battery charging
- Automatic power source selection
- Battery temperature protection
- Pre-charging for deeply discharged batteries
- Accurate charging voltage regulation
- Charging status monitoring with automatic termination
- Sleep mode and system status signaling
By combining battery charging, power-path management, and protection features, the BQTINY-11 module enables reliable power management for compact portable electronic systems.

COMMENTS