* Question
| What are the instructions for using the transformer parameters? |
* Answer
| (1) When replacing the transformer, it is necessary to replace the same type of transformer with the same type of transformer winding structure.For transformer selection during circuit design, !I|0 needs to be optimized for transformer parameters for different applications.In addition, the rated power parameter is also a very important parameter. If the rated power of the selected transformer is small, the transformer will generate heat and affect safety during use.The insulation resistance parameter is a safety indicator. The insulation 够i will cause the power transformer to leak and endanger personal safety. |

COMMENTS