* Question
| What are the key points of the rectifier circuit analysis? |
* Answer
| The diode is mainly used for unidirectional conduction. Only when the voltage on the positive pole of the diode is greater than the voltage on the negative pole, the diode is turned on, otherwise the diode is in the off state.The voltage of the input rectifier circuit is an AC voltage. When the circuit is analyzed, the AC input voltage is divided into a positive half cycle and a negative half cycle.If a positive bias voltage is applied to the diode during one half of the input AC voltage, the other half of the input AC voltage is applied with a reverse bias voltage to the diode. |

COMMENTS