• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • What are the main features of the 82C250?

    * Question

    What are the main features of the 82C250?

    * Answer

    The 82C250 is a specialized integrated circuit (IC) designed by Intel, primarily used as a CAN (Controller Area Network) transceiver. It is part of the 82C2xx series of communication ICs, offering a reliable interface for communication between microcontrollers or microprocessors in industrial and automotive applications. Below are the main features of the 82C250:

    1. CAN Bus Interface
    – Controller Area Network (CAN) Support: The 82C250 is specifically designed for CAN bus communication, allowing for high-speed, reliable communication between embedded systems, controllers, and sensors. It operates according to the ISO 11898 standard for CAN.

    2. Differential Bus Signaling
    – The 82C250 uses differential signaling to communicate with other CAN devices. This allows it to achieve robust communication over long distances (up to 40 meters at 1 Mbps) and in electrically noisy environments, such as automotive and industrial settings.

    3. Low Power Consumption
    – The IC is designed to consume low power while operating, making it suitable for battery-powered or energy-efficient systems.

    4. High-Speed Communication
    – The 82C250 supports high-speed communication up to 1 Mbps, which is essential for many real-time applications requiring fast data transfer, such as automotive control systems, industrial automation, and robotics.

    5. Bus Fault Tolerance
    – The IC has bus fault detection capabilities, including the ability to detect short circuits and other issues in the CAN bus, which helps maintain system reliability and reduces the risk of communication failure.

    6. Slew Rate Control
    – It includes slew rate control, which helps reduce electromagnetic interference (EMI) generated by the switching of the CAN signals, ensuring that the system meets EMC (electromagnetic compatibility) requirements.

    7. Fail-Safe Operation
    – The 82C250 has built-in fail-safe features, ensuring that if the transceiver encounters an issue, it enters a safe state, preventing damage to the system or incorrect communication.

    8. Wide Operating Voltage Range
    – The 82C250 typically operates within a 5V ±10% voltage range, which is compatible with many embedded systems and microcontrollers.

    9. Standby Mode
    – The IC has a low-power standby mode, where it can be placed into a low-power state when communication is not required, further improving power efficiency.

    10. Dominant and Recessive Bit Detection
    – The 82C250 is capable of detecting dominant (logic 0) and recessive (logic 1) bits in the CAN network, allowing it to handle message framing and prioritization.

    11. Integrated Protection
    – The IC is designed to be robust, with built-in protection against over-voltage and electrostatic discharge (ESD), which is critical for automotive and industrial applications.

    12. Compatibility
    – The 82C250 is compatible with various CAN protocol controllers, providing seamless interfacing between the physical layer (transceiver) and the higher layers of the communication stack (e.g., the CAN controller like the 82C200 or other microcontroller-based CAN controllers).

    13. Temperature Range
    – The IC can operate across a wide temperature range, typically from -40°C to +85°C, making it suitable for automotive and industrial environments where temperature extremes are common.

    Typical Applications:
    – Automotive: For engine control, transmission, powertrain, and other subsystems.
    – Industrial Automation: For control systems in factories, robotics, and machinery.
    – Medical Equipment: In devices that require real-time communication.
    – Embedded Systems: For use in embedded applications needing reliable communication protocols.

    Summary
    The 82C250 is an essential component for systems using the CAN bus protocol, providing high-speed, robust communication in environments with electromagnetic interference or other electrical noise. Its features, such as fault tolerance, fail-safe operation, and low power consumption, make it suitable for automotive, industrial, and embedded systems where reliability and real-time data transmission are critical.