* Question
What are the main parameters of the humidity sensitive Resistors? |
* Answer
1.Relative Humidity Relative humidity is the ratio of the actual density of water vapor in the air to the saturation density at the same temperature at a certain temperature, usually expressed as “RH”.For example, 20% RH means that the relative humidity of the air is 20%.4.Humidity measurement range Humidity measurement refers to the humidity measurement of humidity sensitive Resistorss.5.Wet hysteresis effect The hysteresis effect refers to the hysteresis of the electrical parameters of the humidity sensitive Resistors during moisture absorption and desorption. |
COMMENTS