* Question
| What are the main performance characteristics of TJAl040? |
* Answer
| (1) Full compliance with IS011898;
(2) High speed (up to 1 Mb/s); (3) Very low electromagnetic radiation (EME); (4) Differential receiver with a wide common mode range,It has the function of waking up through the bus; (10) transmitting data explicit timeout function; (11) protecting the bus pin in the automotive environment, resisting transient interference; (12) preventing the bus pin and pin SPLIT against the battery and the pairGround short circuit; (13) thermal protection. |

COMMENTS