* Question
| What are the main resource configurations of the OK6410 evaluation board? |
* Answer
| S3C6410 processor, clocked at 533 MHz/667 MHz; 128 MB Mobile DDR memory; 1 GB NAND Flash (MLC); 12 MHz, 48 MHz, 27 MHz, 32. 768 kHz clock source; one reset button with dedicated reset chip; Use 8-bit DIP switch to set the system startup mode; RTC circuit. |

COMMENTS