* Question
| What are the main technical characteristics of the CAT37DC/DC boost converter? |
* Answer
| (1) The low quiescent current is 0.5 mA.
(2) Low resistance (0.5 Ω) power switch, the power efficiency is higher than 80%. (3) Small 5-pin SOT23 (maximum height lmm) and TDFN (maximum height 0.8mm) package, pin configuration compatible with LTl937. |

COMMENTS