* Question
| What are the main technical features of CP2131? | 
* Answer
| (1) Drive up to 3 LEDs with a maximum current of 30mA per LED.
 (2) The current matching accuracy is 0.5% (typical). (3) Auto-Mirror technology ensures the current matching degree under the condition that the voltage difference between the parallel white LEDs is large.(9) With over current protection and overheat protection. (10) Operating voltage range: 2.7 ~ 5.5V. (11) It is packaged in a small 3mm × 3mm QFNl6L package.  | 

COMMENTS