• Home
  • QUESTIONS & ANSWERS
  • Industrial Controls, Meters
  • What are the precautions for using the pulse output command PLS/PLF?

    * Question

    What are the precautions for using the pulse output command PLS/PLF?


    *
    Answer

    (1) PLS is the pulse rising edge differential output command, and PIJ is the pulse falling edge differential output command.The PLS and PLF commands can only be used for output relay Y and auxiliary relay M (excluding special auxiliary relays).

    (3) When the input relay X0 is turned on, the PLS M0 command will output a pulse when the PIKE is operated by the stop.However, if a battery backup/latch auxiliary relay is used instead of M0, its PLS command will not output a pulse in this case.


    COMMENTS

    WORDPRESS: 0
    DISQUS: 0