* Question
| What are the principles to follow for antenna selection? |
* Answer
| 1) Determine the density of different antenna hanging points according to the different building scenarios. For example, in an open environment, an antenna is placed at intervals of 15 to 20 m; in a glass-shielded scene, an antenna is placed at 10 to 15 m;Place an antenna at ~11m; place an antenna in the scene of 4~8m blocked by concrete wall.
5) For indoor scenes with complex internal structures, multi-point coverage of small power antennas should be used to avoid the effects of shadow fading and wall wear. 6) For buildings that require indoor and outdoor wireless coverage, determine whether the outdoor ground, building surface, and building walls have suitable locations for antenna deployment. |

COMMENTS