* Question
| What are the representative products of DSP processors? |
* Answer
| The representative products of the DSP processor are TI’s TMS320 series and Freescale’s DSP56000 series.The TMS320 family of processors includes the C2000 series for control, the C5000 series for mobile communications, and the higher performance C6000 and C8000 series.In addition, PHILIPS has also introduced R., which is based on a resettable embedded DSP structure and manufactured using low-cost, low-power technology.E.A.The L DSP processor features dual Harvard architecture and dual-multiply/accumulate units for high-volume consumer products. |

COMMENTS