* Question
| What are the Resistorss allowed for error representation? |
* Answer
| There are three ways to indicate the allowable error of the Resistors.
(1) Directly expressed in %. (2) Expressed by letters.Table l.Listed in 3 is the specific meaning of the Resistors error tolerance letter. (3) It is represented by I, Il, and IIl.I represents ±5%, 11 represents ±10%, and IIl represents ±20%. |

COMMENTS