* Question
What are the routing algorithms for filtering injection nodes based on utility functions?
* Answer
Routing algorithms that filter injection nodes based on utility functions are typically used in network optimization, wireless sensor networks, on-chip networks (NoCs), and ad hoc communication systems. These algorithms aim to select the best source or relay nodes (i.e., injection points for data into the network) by evaluating a utility function that quantifies node performance, resource availability, or network goals.
Table of Contents
ToggleCore Concept: Utility-Based Routing
A utility function evaluates each candidate node (injection node) based on multiple metrics, such as:
Residual energy (in sensor networks)
Queue length / buffer availability
Link quality or reliability
Proximity to destination
Congestion level or delay
Application-level QoS parameters
Nodes with higher utility scores are preferred for routing or injection.
Common Routing Algorithms Using Utility Functions
1. Utility-Based Adaptive Routing
Principle: Dynamically evaluates each possible injection node using a utility function.
Mechanism:
Each node calculates its utility score.
Only nodes with utility above a threshold are selected for packet injection.
Application: Network-on-Chip (NoC) and data center fabrics to reduce congestion and increase throughput.
2. Reinforcement Learning-Based Routing
Principle: Nodes learn and update their utility scores over time based on feedback.
Mechanism:
Q-values or rewards are used as utility.
Routing decisions are based on maximizing long-term utility.
Example: Q-routing, Deep Q-networks in wireless mesh or UAV networks.
3. Opportunistic Routing with Utility Filtering
Principle: Chooses the best injection node among candidates at runtime.
Mechanism:
A utility function ranks neighbor nodes.
A candidate list is created based on a utility threshold or top-k selection.
Packets are injected through nodes with the highest scores.
Use Case: Mobile ad hoc networks (MANETs), Delay-Tolerant Networks (DTNs).
4. Backpressure-Based Routing with Utility Metrics
Principle: Routing decisions based on differential backlogs (queue lengths).
Extended Idea: Combine backlog with other metrics (e.g., link quality) to compute utility.
Filtering: Nodes with low combined utility are excluded from injection.
5. Multi-Criteria Decision Making (MCDM) in Routing
Uses techniques like AHP, TOPSIS, or Fuzzy Logic to evaluate multiple metrics as part of a composite utility function.
Filtering is applied to eliminate nodes that don’t meet minimum thresholds across criteria.
Generic Utility Function Example
U(i)=α⋅Ri+β⋅Qi+γ⋅LQi
Where:
Ri: residual energy or resource level
Qi: inverse of queue length or congestion
LQi: link quality metric
α,β,γ: weights based on application priorities
Only injection nodes with U(i)>θ are considered in the routing path.
Summary of Use Cases
Algorithm Type | Filtering Basis | Application Domains |
Adaptive Utility Routing | Thresholding utility values | NoC, wireless networks |
RL-based Routing | Learned Q-values as utility | Mesh networks, UAV routing |
Opportunistic Routing | Best-k node selection | MANET, VANET, IoT |
Backpressure + Utility | Queue + performance metrics | Data center routing, wireless sensor networks |
MCDM Utility Filtering | Weighted multi-metric ranking | Smart grids, IoT, disaster recovery networks |

COMMENTS