* Question
| What are the SPI interface features? |
* Answer
| The SPI interface features are as follows:
(1) with two fully independent SPI controllers; (2) following the Synchronous Serial Interface (SPI) specification; (3) full-duplex data communication; (4) configurable as SPI master or slave (5) The maximum data bit rate is 1/8 of the peripheral clock FPCLK. |

COMMENTS