* Question
| What are the two major advantages of ANT? |
* Answer
| ANT has two major advantages: First, the power consumption is extremely low, and the minimum anal A can reach 5 anus in sleep. It can be used for several years of working life with button battery.Similar to low-power Bluetooth, the peak current of the ANT operating state is only 10-20 mA, while the standard Bluetooth is 50-100 mA and the WiFi is hundreds of mA.With proper configuration, a node in the network can belong to different networks at the same time, and it can be either a master node or a slave node on different channels. |

COMMENTS