* Question
What events are generated when the information is exchanged between entities?
* Answer
When information is exchanged between entities—such as devices, processes, or network nodes—a series of protocol-driven and system-level events are generated. These events represent different stages of communication and are essential for managing synchronization, data integrity, error handling, and resource coordination.
The exact set of events depends on the communication model (e.g., OSI model, TCP/IP stack, or distributed message-passing architecture), but generally, the following key event types are involved:
Table of Contents
Toggle1. Connection Establishment Events
These events occur when communication is initialized between two entities:
Connection Request (CONNECT_REQ): Initiated by the sending entity to establish a session or link.
Connection Acknowledgment (CONNECT_ACK): The receiving entity acknowledges and agrees to the session.
Session Start Event: Signals that a logical communication channel is active.
Example: In TCP, this corresponds to the SYN/SYN-ACK/ACK handshake.
2. Data Transfer Events
These represent the actual transmission of data and acknowledgment of receipt:
Data Sent Event (DATA_REQ): Indicates that a data frame or packet has been transmitted.
Data Received Event (DATA_IND): Signifies that data has been received at the destination.
Acknowledgment Event (ACK_IND): Confirms successful receipt of data, often used in reliable protocols.
These events enable flow control and buffer management in the communicating systems.
3. Error and Exception Events
Generated when issues arise during transmission:
Transmission Error Event: Triggered by checksum mismatch, timeouts, or line noise.
Retransmission Request (RETRANS_REQ): Initiated by a receiving entity in case of missing or corrupt data.
Protocol Violation Event: Occurs if the data exchange violates protocol rules.
4. Control and Synchronization Events
These help manage the state and sequencing of the communication:
Flow Control Event: Throttles data rate based on receiver buffer capacity.
Sequence Number Event: Ensures in-order delivery of frames or packets.
Window Update Event: In sliding window protocols, signals changes in receiver window size.
5. Disconnection Events
Generated when communication is terminated:
Disconnect Request (DISCONNECT_REQ): One entity requests session termination.
Disconnect Confirmation (DISCONNECT_CONF): Acknowledges and confirms termination.
Session Closed Event: Indicates that resources tied to the session are released.
Example: In TCP, this aligns with FIN/ACK exchange and socket teardown.
In Summary:
When information is exchanged between entities in a digital communication environment, events are generated at multiple layers to track:
Connection establishment and teardown,
Data transmission and acknowledgment,
Error detection and correction,
Flow control and synchronization.
These events form the backbone of protocol management and ensure reliable, orderly, and efficient communication between distributed components.

COMMENTS