* Question
What is a two-stage operational amplifier?
* Answer
A two-stage operational amplifier (op-amp) is a commonly used analog circuit architecture that consists of two primary amplification stages, designed to provide high gain, wide bandwidth, and good performance in feedback systems such as analog signal processing, data converters, and active filters.
Table of Contents
ToggleStructure of a Two-Stage Op-Amp
First Stage: Differential Amplifier
Purpose: Provides the input differential gain and common-mode rejection.
Key components:
A pair of transistors forming a differential pair.
A current mirror as an active load, which helps in achieving high gain.
Biasing circuitry to establish the desired operating point.
Second Stage: Common-Source/Emitter Amplifier
Purpose: Provides additional gain and voltage swing.
Often implemented as a common-source (MOSFET) or common-emitter (BJT) amplifier.
Typically, the second stage has a high output impedance, which is suitable for driving loads or next stages.
Key Features
High Voltage Gain: Product of gains from both stages.
Improved Swing and Drive Capability: Especially in the second stage.
Common-Mode Rejection Ratio (CMRR): Enhanced by the differential first stage.
Phase Margin and Stability: Requires frequency compensation, often through Miller compensation, to ensure stable operation when used in negative feedback loops.
Common Applications
Analog-to-digital and digital-to-analog converters.
Signal conditioning circuits.
Active filters and oscillators.
Voltage regulators and control systems.
Example: Miller-Compensated Two-Stage Op-Amp
In this classic architecture:
A compensation capacitor (typically connected between the output of the first stage and the input of the second) introduces a dominant pole to ensure stability.
A nulling resistor or current buffer might be added to enhance phase margin.

COMMENTS