* Question
| What is an AC motor? |
* Answer
| A power source that converts electrical energy into mechanical energy.Like a DC motor, an AC motor is also composed of a stator and a rotor.The stator is mainly composed of a stator core and a stator winding, and is a stationary part of the motor for generating a rotating magnetic field.2) Working principle of AC motor Like the DC motor, the AC motor is also rotated by the force in the magnetic field in the rotor winding. |

COMMENTS